Other Parts Discussed in Thread: TMS470MF06607
I have an application running on the TMS470MF06607 that uses two SCI ports. One is configured for ~105k baud 8n1 and the other is configured for ~10.4k baud 9n2. The main clock is 10MHz and SCI1/SCI2, which are source from VCLK1, are sourced at 5MHz.
Here is the SciInit function for reference:
void SciInit(void)
{
// --------------------SCI 1:APP-----------------------
sciREG1->GCR0 = 1U;
sciREG1->CLRINT = 0xFFFFFFFFU;
sciREG1->CLRINTLVL = 0xFFFFFFFFU;
sciREG1->GCR1 = (1U << 25U) /* enable transmit */
| (1U << 24U) /* enable receive */
| (1U << 5U) /* internal clock */
| (2U << 4U) /* number of stop bits */
| (1U << 1U) /* asynchronous timing mode */
| (1U); /* address-bit mode */
sciREG1->BRS = 29U; // baud = 10417
sciREG1->FORMAT = 7U; // length
sciREG1->FUN = (1U << 2U) | (1U << 1U);
sciREG1->DOUT = 0U;
sciREG1->DIR = (1U << 2U);
sciREG1->ODR = 0U;
sciREG1->PD = (1U << 2U) | (1U << 1U);
sciREG1->PSL = 1U;
sciREG1->SETINT = (1U << 9U); // Rx
sciREG1->SETINTLVL = 0U;
sciREG1->GCR1 |= (1U << 7U);
// --------------------SCI 2:DEBUG-----------------------
sciREG2->GCR0 = 1U;
sciREG2->CLRINT = 0xFFFFFFFFU;
sciREG2->CLRINTLVL = 0xFFFFFFFFU;
sciREG2->GCR1 = (1U << 25U) /* enable transmit */
| (1U << 24U) /* enable receive */
| (1U << 5U) /* internal clock */
| (1U << 4U) /* number of stop bits */
| (1U << 1U); /* asynchronous timing mode */
sciREG2->BRS = 2U; // baud = ~105000
sciREG2->FORMAT = 7U; // length
sciREG2->FUN = (1U << 2U) | (1U << 1U);
sciREG2->DOUT = 0U;
sciREG2->DIR = 0U;
sciREG2->ODR = 0U;
sciREG2->PD = 0U;
sciREG2->PSL = (1U << 2U) | (1U << 1U) | (1U);
sciREG1->SETINT = 0U;
sciREG1->SETINTLVL = 0U;
sciREG2->GCR1 |= (1U << 7U);
}
As you can see, SCI1 is the 9bit application port that is configured to interrupt on RX. SCI2 is a debug port I use to output state information and error messages.
The problem I'm having is that when I run my code attached to the debugger it works fine. When I disconnect the debugger, it continues to work. But if I power cycle the device the code all runs but the RX interrupt on SCI1 stops working.
Here are other things I've tried and notes about the situation:
- I'm using CCS v6.0
- I'm using an XDS100V2 and physically connecting or disconnecting it does not solve the problem
- I've tried changing the optimization level from none to highest -- no change
- I've monitored the POR and RST lines during debug and when it's disconnected and there is no change, though it should not make a difference because I know the code is running
- When disconnected from debug and power cycled the transmit for both SCI1 and SCI2 work fine, but are not interrupt driven
- I've monitored VCLK by redirecting it to ECLK and looking at it on a scope, when in debug or power cycled the clock is solid
- I've checked signal integrity of the RX line on the device PCB and it appears unchanged whether in debug or not
- If I power cycle then attach the debugger without resetting or reprogramming the device (attach to a running target) then the interrupt will start working
- I've tried building in debug/release modes and the outcome is the same
Any help would be appreciated -- this is a pretty interesting and frustrating problem.