This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCI transmit adds a "1" bit at the end of character in TMS570LS1227

In SCI multibuffer mode, when I transmit a set of characters, the first character is transmitted correctly, then subsequent characters have an extra "1" bit tagged on to the end of the stream. The Stop and Start bits are normal, parity is not enabled.