Other Parts Discussed in Thread: HALCOGEN
Using HALCoGen Version 4:
The FEE driver generates the following file:
./include/ti_fee_Cfg.h
In file fee_interface.h, also generated by the HALCoGEn FEE driver, we have the following include:
#include "ti_fee_cfg.h"
This creates an issue on linux and unix, because on these OS the file "ti_fee_cfg.h" is not the same as "ti_fee_Cfg.h".
You can temporary solve that by renaming the file or changing the include, but a new code generation cycle from HALCoGen may create issues.
I have temporarily solved this by creating the following symbolic link in the include directory:
ln -s ti_fee_Cfg.h ti_fee_cfg.h
This is not an issue on Windows, where the filenames are not case sensitive.