Other Parts Discussed in Thread: HALCOGEN
I could be missing something obvious here but I have been testing the NHET on the RM48L950PGE. I have set up PWM0 on NHET01[04] and loaded a simple routine that allows me to modify the duty cycle and period.
As you can see below the waveform for duty cycle 50% and period of 1 second (1000000usecs) looks correct.
If I try to change this to a period of 2 seconds (0.5Hz) the duty cycle becomes 25% as opposed to longer 50% pulse:
Here is the code, I vary pwm0_signal elements in the debug window to change the waveform
void main(void)
{
/* USER CODE BEGIN (3) */
hetInit();
pwm0_enb = false;
pwm0_signal.duty = 50;
pwm0_signal.period = 1000; /*in usecs*/
while(1)
{
if(pwm0_enb)
{
/*pwmSetDuty(hetRAM1,pwm0,pwm0_duty);*/
pwmSetSignal(hetRAM1,pwm0,pwm0_signal);
pwmStart(hetRAM1,pwm0);
}
else
{
pwmStop(hetRAM1,pwm0);
}
/* Forever */
}
/* USER CODE END */
}