Other Parts Discussed in Thread: TM4C123GH6PZ
Hi...I'm new to TM4C123GH6PZ (tivaware series)..my first program is toggling the LED.and i'm checking the frequency through oscilloscope.n crystal frequency is 8Mhz.
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
//uint8_t ui8PinData=2;
int main(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_1|SYSCTL_USE_OSC|SYSCTL_XTAL_8MHZ|SYSCTL_OSC_MAIN);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7);
while(1)
{
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7, 0xff);
SysCtlDelay(2);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7, 0x00);
SysCtlDelay(2);
//if(ui8PinData==8) {ui8PinData=2;} else {ui8PinData=ui8PinData*2;}
//}
}
}
i have set 8Mhz as an system clock.when i have checked in ossciloscope m getting 800.1k..