This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FreeRTOS 8.0 DEMO with RM48 HDK



Hi.

I'm Wonjae

I'm using RM48 HDK. I found demo project in FreeRTOS 8.0.

That project name is 'CORTEX_R4_RM48_TMS570_CCS5' in 'FreeRTOSV8.0.0/FreeRTOS/Demo'

I tried it to build with 'RM48 with FPU' mode. But It makes some errors that has no name in portASM.asm.

So I changed Runtime support library rtsv7R4_T_le_v3D16_eabi.lib and compiler version TI v 4.9.7.

And then those errors are disappeared. but new error occured

"unresolved symbol __clz, first referenced in ./FreeRTOS/tasks.obj"

I tried CCS 5.5 and 6.0.

Please help with this problem.

Thank you in advance