Other Parts Discussed in Thread: RM57L843, RM48L952, HALCOGEN
While migrating my project from an RM48L952 using ARM tools in HALCoGen 3.06.00, to an RM57L843 in HALCoGen 4.00.00; I noticed the following:
1) On the RM57L843ZWT tab, the block diagram on the General tab is labeled "RM57L643 Block Diagram", and some blocks, such as DMA, are greyed out. Though the RM57L643 is the wrong processor, will HalCoGen still produce the correct drivers for the RM57L843 device as selected when the project is created?
2) Under View->Device Explorer, the device explorer shows the TMS570LC4357ZWT. Again, as the wrong processor, will this still generate the correct drivers for the RM57L843?
3) When creating the project, there are no options to select "ARM Tools". My project requires the use of an ARM compiler. Will an "ARM Tools" selection be available in the future?
Thanks,
Dan