The version used by lwip by TI is rather old at this point. I'd like to update to the latest version. Can anybody help with that - in particular, point out the important driver code that interfaces with lwip?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The version used by lwip by TI is rather old at this point. I'd like to update to the latest version. Can anybody help with that - in particular, point out the important driver code that interfaces with lwip?
Thanks
Michael Hu. said:The version used by lwip by TI is rather old at this point. I'd like to update to the latest version. Can anybody help with that - in particular, point out the important driver code that interfaces with lwip?
Latest LWIP is 1.4.1
TI is using release 1.4.1
Please can you point us where are newest version of LWIP?
I am programming on the ARM-M3 core on the F28M35x, and the lwip code there is version 1.3.2. Perhaps this is the wrong forum?
Michael Hu. said:I am programming on the ARM-M3 core on the F28M35x, and the lwip code there is version 1.3.2. Perhaps this is the wrong forum?
Yes, concerto is a C2000 dual core member so you can repost your question there:
http://e2e.ti.com/support/microcontrollers/c2000/f/171.aspx
TIVA is series TM4C12xx of cortex M4
Michael Hu. said:F28M35x
The appropriate forum for this microcontroller is at the Concerto Forum. See, link below.
http://e2e.ti.com/support/microcontrollers/c2000/default.aspx
-kel
Markel Robregado said:The appropriate forum for this microcontroller is at the Concerto Forum. See, link below.
Independent dual processing parallel post ;)
@Roberto
I missed reading your reply. I replied that early in the morning and half-awake.
-kel
Markel Robregado said:I missed reading your reply. I replied that early in the morning and half-awake.
Markel, see more close to post, where impossible to both read the post we wrote, are at the same time ;)