Other Parts Discussed in Thread: TM4C123GH6PM, LM324
Hello Everybody,
I am Sreenivasa S, working as SE in XXX company, I am using the TIva C series MCU(TM4C123GH6PM) for reducing the size of the image.
our need:
API which reduces the image size depending on the input parameter. EX: if we have 1MB image file as input then output should be of either 500KB image(50% of original image) or 250KB(25% of original image) depending upon the input parameters to the API.
I searched for API, but I could not get any source code for our requirement, If any one has an idea or the open source please share with me. I will be much thankful. Even though exact source code not available please help me some algorithms which I can use...
Thanks in advance...
Sreenivasa.