Other Parts Discussed in Thread: TMS570LS3137
Hi.
My question is regarding the TMS570LS3137.
In spns162b.pdf, page 96 are also the following two ESM channel assignments stated:
* DMA/DMM - imprecise read error, Group1, channel 5
* DMA/DMM - imprecise write error, Group1, channel 13
I generate the DMA imprecise read error, by a DMA-read access from an unimplemented address (using DMA channel 4). I observe that the bit 5 in the ESM register ESMSR1 (i.e. ESMSR1.5) will be set to 1. BUT I cannot observe that the bit 4 in the DMA register BERFLAG (i.e. BERFLAG.4) will be set (Reason why bit 4: Since DMA channel 4 is used.).
I generate the DMA imprecise write error, by a DMA-write access to an unimplemented address (using DMA channel 5). I observe that the bit 13 in the ESM register ESMSR1 (i.e. ESMSR1.13) will be set to 1. BUT I cannot observe that the bit 5 in the DMA register BERFLAG (i.e. BERFLAG.5) will be set (Reason why bit 5: Since DMA channel 5 is used.).
Several notes:
* Note 1: I've tried it with DMA interrupts enabled and disabled, i.e.:
- GCHIENAS.4 = GCHIENAS.5 = 1
- GCHIENAS.4 = GCHIENAS.5 = 0
But I observed no difference.
* Note 2: DMA register BERMAP = 0.
* Note 3: In case a DMA - MPU error will be generated (i.e. ESM channel "DMA - MPU", Group1, channel 2), I observe the following:
- The bit 2 in the ESM register ESMSR1 (i.e. ESMSR1.2) will be set to 1.
- The corresponding bit in DMA register BERFLAG will also be set to 1.
So my question is: Why will the corresponding bits in DMA register BERFLAG not be set in case of a DMA - imprecise read/write error?
Regards
Oliver.