This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where do I find USB0DeviceIntHandler?



I am learning to use TiVa 1294 kit

All USB-based examples has this "extern void USB0DeviceIntHandler(void);" in its startup_ccs.c,  but when I want to read more into this, I can't find its source.

Any pointer?

Thanks!

  • Hello David,

    The Interruot Handler and it's function call is in the TIVAWare usblib directory

    For device specific it is in

    C:\ti\TivaWare_C_Series-2.1.0.12573\usblib\device

    Regards

    Amit

  • Got it, Thanks, Amit,

    CCS doesn't provide a way to search all the source files under a project, so I used my old CodeWright to search the project directory, but it didn't work properly under Windows 7 due to bad configuration :)

  • Amit, need your pointer again, 

    I tried to add test points inside USB0DeviceIntHandler since my design requires hooking to the USB rx routine in the lowest level to minimize the software latency, but no matter what I do, including to totally messing up the codes (changing USB0DeviceIntHandler to USB0DeviceIntHandler2!) , the projects ignores my modifications. 

    What did I miss here?

    Thanks for your reply in advance!

  • Hello David

    Did you modify the startup_ccs.c file to change the mapping to the new device interrupt handler?

    Otherwise you would need to use

    IntDisable(INT_USB0);

    IntRegister(INT_USB0,USB0DeviceIntHandler2);

    IntEnable(INT_USB0);

    The former suggestion would work though

    Regards

    Amit

  • I'v tried that already, and it didn't help. I got a feeling the linker is pulling a .lib or .obj from outside of my project even though I had changed the codes insides usblib

    Maybe CCS doesn't work properly under Windows 7, since I keep getting notice like the following --- wrong date may prevent the linker and compiler to realize I have changed the files.

    **** Build of configuration Debug for project watchdog ****

    "C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
    gmake: ../startup_ccs.c: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: ../watchdog.c: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: ../watchdog_ccs.cmd: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: Nothing to be done for `all'.

    **** Build Finished ****

  • Hello David,

    Can you zip your project and send it across? I may have to check the project database.

    Also which version of CCS and TIVAWare are you using?

    Regards

    Amit

  • Amit, thanks for your reply.

    I have an urgent product release next week, so I will get back to you later after that

  • 1057.enet_lwip.zip

    It seems all example projects have this TimeStamp issue.... to avoid confusion, I attached one from TI's example project (enet_lwip) without any modification:

    "C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 

    gmake: ../enet_fs.c: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: C:/Users/Chen/TiVa/enet_lwip/lwipopts.h: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: ../enet_fsdata.h: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: ../enet_lwip.c: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: ../startup_ccs.c: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: ../enet_lwip_ccs.cmd: Timestamp out of range; substituting 1969-12-31 19:00:00
    gmake: Nothing to be done for `all'.

    Thanks for your time!