Other Parts Discussed in Thread: STRIKE
Dear sir/madam
I am trying to write a code to transfer a part of memory to other location in memory by DMA and external trigger signal. I choose PORTE_PIN_3 as a trigger signal to DMA and I have connected an external square wave to this pin. Also I assigned DMA in UDMA_CH14_GPIOE and I have used ping pong mode but I monitored the memory there was not any data transfer. Could you please help me to figure out where the problem is?
The written code is as following.
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/udma.h"
#include "driverlib/PWM.h"
#include "driverlib/rom_map.h"
// Buffer definitions
#define UART_TXBUF_SIZE 16
#define UART_RXBUF_SIZE 16
static uint8_t g_pui8TxBuf[UART_TXBUF_SIZE];
static uint8_t g_pui8RxPing[UART_RXBUF_SIZE];
static uint8_t g_pui8RxPong[UART_RXBUF_SIZE];
void PWMInit1(void);
// Error counter
static uint32_t g_ui32DMAErrCount = 0;
// Transfer counters
static uint32_t g_ui32RxPingCount = 0;
static uint32_t g_ui32RxPongCount = 0;
// uDMA control table aligned to 1024-byte boundary
#pragma DATA_ALIGN(ucControlTable, 1024)
uint8_t ucControlTable[1024];
// Library error routine
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
// uDMA error handler
void
uDMAErrorHandler(void)
{
uint32_t ui32Status;
ui32Status = ROM_uDMAErrorStatusGet();
if(ui32Status)
{
ROM_uDMAErrorStatusClear();
g_ui32DMAErrCount++;
}
}
// UART interrupt handler. Called on completion of uDMA transfer
void
DMA1IntHandler(void)
{
uint32_t ui32Status;
uint32_t ui32Mode;
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, GPIO_PIN_1);
// ui32Status = ROM_UARTIntStatus(UART1_BASE, 1);
GPIOIntClear(GPIO_PORTE_BASE, GPIO_PIN_3);
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CH14_GPIOE | UDMA_PRI_SELECT);
if(ui32Mode == UDMA_MODE_STOP)
{
g_ui32RxPingCount++;
ROM_uDMAChannelTransferSet(UDMA_CH14_GPIOE | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
g_pui8TxBuf+2,
g_pui8RxPing, sizeof(g_pui8RxPing));
}
ui32Mode = ROM_uDMAChannelModeGet(UDMA_CH14_GPIOE | UDMA_ALT_SELECT);
if(ui32Mode == UDMA_MODE_STOP)
{
g_ui32RxPongCount++;
ROM_uDMAChannelTransferSet(UDMA_CH14_GPIOE | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(g_pui8TxBuf),
g_pui8RxPong, sizeof(g_pui8RxPong));
}
if(!ROM_uDMAChannelIsEnabled(UDMA_CH14_GPIOE))
{
ROM_uDMAChannelTransferSet(UDMA_CH14_GPIOE | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
g_pui8TxBuf,
g_pui8RxPing, sizeof(g_pui8RxPing));
ROM_uDMAChannelEnable(UDMA_CH14_GPIOE);
}
}
// Initialize UART uDMA transfer
void
InitDMATransfer(void)
{
uint32_t ui32Idx;
// Initialize transmit buffer with some data
for(ui32Idx = 0; ui32Idx < UART_TXBUF_SIZE; ui32Idx++)
{
g_pui8TxBuf[ui32Idx] = ui32Idx;
}
// Enable UART1 and make sure it can run while the CPU sleeps
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_GPIOE);
// Configure and enable the UART with DMA
ROM_GPIOPinTypeGPIOInput(GPIO_PORTE_BASE,GPIO_PIN_3);
ROM_GPIOIntTypeSet(GPIO_PORTE_BASE,GPIO_PIN_3, GPIO_RISING_EDGE);
ROM_GPIOPadConfigSet(GPIO_PORTE_BASE,GPIO_PIN_3,GPIO_STRENGTH_8MA,GPIO_PIN_TYPE_STD_WPD);
GPIOIntClear(GPIO_PORTE_BASE, GPIO_PIN_3);
ROM_GPIODMATriggerEnable(GPIO_PORTE_BASE, GPIO_PIN_3);
GPIOIntEnable(GPIO_PORTE_BASE, GPIO_PIN_3);
ROM_IntEnable(INT_GPIOE);
IntMasterEnable();
// Receive channel setup for ping and pong
ROM_uDMAChannelAttributeDisable(UDMA_CH14_GPIOE,
UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
UDMA_ATTR_HIGH_PRIORITY |
UDMA_ATTR_REQMASK);
ROM_uDMAChannelControlSet(UDMA_CH14_GPIOE | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 | UDMA_DST_INC_8 |
UDMA_ARB_8);
ROM_uDMAChannelControlSet(UDMA_CH14_GPIOE | UDMA_ALT_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 | UDMA_DST_INC_8 |
UDMA_ARB_8);
ROM_uDMAChannelTransferSet(UDMA_CH14_GPIOE | UDMA_PRI_SELECT,
UDMA_MODE_PINGPONG,
g_pui8TxBuf+2,
g_pui8RxPing, sizeof(g_pui8RxPing));
ROM_uDMAChannelTransferSet(UDMA_CH14_GPIOE | UDMA_ALT_SELECT,
UDMA_MODE_PINGPONG,
(g_pui8TxBuf+2),
g_pui8RxPong, sizeof(g_pui8RxPong));
// Transmit channel setup for a basic transfer
// Enable both channels
ROM_uDMAChannelEnable(UDMA_CH14_GPIOE);
// ROM_uDMAChannelRequest(UDMA_CH14_GPIOE);
}
// main code
int
main(void)
{
volatile uint32_t ui32Loop;
ROM_FPULazyStackingEnable();
ROM_SysCtlClockSet(SYSCTL_SYSDIV_64 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
ROM_SysCtlPeripheralClockGating(true);
// GPIO setup for LEDs
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2 | GPIO_PIN_1);
// Enable uDMA
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
ROM_SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
ROM_IntEnable(INT_UDMAERR);
ROM_uDMAEnable();
ROM_uDMAControlBaseSet(ucControlTable);
// Initialize the uDMA/UART transfer
InitDMATransfer();
// PWMInit1();
// Blink the LED while the transfers occur
while(1)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2, GPIO_PIN_2);
SysCtlDelay(SysCtlClockGet() / 20 / 3);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0);
SysCtlDelay(SysCtlClockGet() / 20 / 3);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1, 0);
}
}