Hi, how can I set PLL config to get max? the default is 300 Mhz (16/8/150) but I'd like to get 330 Mhz.
Thanks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, how can I set PLL config to get max? the default is 300 Mhz (16/8/150) but I'd like to get 330 Mhz.
Thanks~
Hi Young,
You can use the PLL configuration tool available at
http://www.ti.com/lsds/ti/arm/hercules_arm_cortex_r_safety_microcontrollers/arm_cortex_r4/rm4_arm_cortex_r4/toolsw.page#add (http://www.ti.com/tool/fmzpll_calculator)
But when you configure the CPU clock to 330 MHz pls try to make sure you get the fHCLK <=150 MHz using the BUS1CNTRL divider configuration. So when GCLK=330MHz you can go with HCLK(max)=110MHz.