Other Parts Discussed in Thread: TM4C129XNCZAD
Hello Experts,
I am using TM4C129XNCZAD micro-controller, I have to send data in packets of 20 bytes and data bytes must follow some hard-coded macro such as 0xFF05. So, I have written a code which looks some thing like this
Cmd_Length = Int_length;
while(Cmd_Length != 0)
{
if(Cmd_Length > p_len)
{
while((GPIO_PORTM_DATA_R & 0x80) == 0); //Check for pin to go low
UARTSend(HANDLE_WS_UPGRADE_DATA,2);
UARTSend(p_len,1);
UARTSend(0x000000,3);
for(ui32Loop = 0; ui32Loop < 20; ui32Loop++)
{
UARTCharPut(UART0_BASE,*q++);//(Local_Buffer[ui32Loop],1);
}
}
else
{
while((GPIO_PORTM_DATA_R & 0x80) == 0);
UARTSend(HANDLE_WS_UPGRADE_DATA,2);
UARTSend(Cmd_Length,1);
UARTSend(0x000000,3);
for(ui32Loop = 0; ui32Loop < Cmd_Length; ui32Loop++)
{
UARTCharPut(UART0_BASE,*q++);//(Local_Buffer[ui32Loop],1);
for(i=0; i<9000000; i++)
{
}
}
Cmd_Length = 20;
} Cmd_Length = (Cmd_Length - p_len);
}
In this code the three lines highlighted above are skipped after first itretion of the loop.
please anyone suggest any solution!!!