Hi, I'm using CCSv6 and wrote some codes based on the Launchpad Workshop Lab 15.
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/debug.h"
#include "driverlib/pwm.h"
#include "driverlib/pin_map.h"
#include "inc/hw_gpio.h"
#include "driverlib/rom.h"
#define PWM_FREQUENCY 200
int main(void) {
volatile uint32_t ui32Load;
volatile uint32_t ui32PWMClock;
volatile int32_t i32DutyCycle = 500;
// Run at 40 MHz
ROM_SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
// Set PWM clock at 40e6/64 = 625 kHz
ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
// Enable M1PWMx
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
// Enable port F for PF4 (SW1), PF0 (SW2), PF2 (M1PWM6), PF3 (M1PWM7)
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
// Set PF2 and PF3 as PWM output pins
ROM_GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_2|GPIO_PIN_3);
// Configure PF2 as M1PWM6, and PF3 as M1PWM7
ROM_GPIOPinConfigure(GPIO_PF2_M1PWM6|GPIO_PF3_M1PWM7);
// Unlock the GPIO commit control register (for PF0)
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01;
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0;
// Set PF4 (SW1) and PF0 (SW2) as input pulled-up
ROM_GPIODirModeSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_DIR_MODE_IN);
ROM_GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
ui32PWMClock = ROM_SysCtlClockGet() / 64;
// Load = 625000/20 - 1 = 31249 ticks
ui32Load = (ui32PWMClock / PWM_FREQUENCY) - 1;
// Configure M1PWM6 and M1PWM7 as a down-counter (count to zero)
ROM_PWMGenConfigure(PWM1_BASE, PWM_GEN_3, PWM_GEN_MODE_DOWN);
ROM_PWMGenPeriodSet(PWM1_BASE, PWM_GEN_3, ui32Load);
// Set the pulse-width (# of clock ticks)
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6, ui32Load*i32DutyCycle/1000);
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_7, ui32Load - ui32Load*i32DutyCycle/1000);
// Enable the outputs
ROM_PWMOutputState(PWM1_BASE, PWM_OUT_6_BIT|PWM_OUT_7_BIT, true);
ROM_PWMGenEnable(PWM1_BASE, PWM_GEN_3);
while(1)
{
if(ROM_GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_4) == 0x00)
{
i32DutyCycle --;
if (i32DutyCycle < 0)
{
i32DutyCycle = 0;
}
}
if(ROM_GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_0) == 0x00)
{
i32DutyCycle ++;
if (i32DutyCycle > 999)
{
i32DutyCycle = 999;
}
}
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6, ui32Load*i32DutyCycle/1000);
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_7, ui32Load - ui32Load*i32DutyCycle/1000);
ROM_SysCtlDelay(20e3);
}
}
The first problem is that only the green LED on PF3 works. The blue LED on PF2 never lit up.
Also, when I use "non-ROM" functions, such as changing ROM_SysCtlClockGet() to SysCtlClockGet(), there will be a compilation failure.
**** Build of configuration Debug for project PWM_test **** "c:\\ti\\ccsv6\\utils\\bin\\gmake" -k all 'Building file: ../main.c' 'Invoking: ARM Compiler' "c:/ti/ccsv6/tools/compiler/arm_5.1.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="c:/ti/ccsv6/tools/compiler/arm_5.1.6/include" --include_path="C:/ti/TivaWare_C_Series-2.1.0.12573" -g --define=PART_TM4C123GH6PM --define=TARGET_IS_BLIZZARD_RB1 --display_error_number --diag_warning=225 --diag_wrap=off --preproc_with_compile --preproc_dependency="main.pp" "../main.c" 'Finished building: ../main.c' ' ' 'Building target: PWM_test.out' 'Invoking: ARM Linker' "c:/ti/ccsv6/tools/compiler/arm_5.1.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -g --define=PART_TM4C123GH6PM --define=TARGET_IS_BLIZZARD_RB1 --display_error_number --diag_warning=225 --diag_wrap=off -z -m"PWM_test.map" --heap_size=0 --stack_size=512 -i"c:/ti/ccsv6/tools/compiler/arm_5.1.6/lib" -i"c:/ti/ccsv6/tools/compiler/arm_5.1.6/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="PWM_test_linkInfo.xml" --rom_model -o "PWM_test.out" "./tm4c123gh6pm_startup_ccs.obj" "./main.obj" "../tm4c123gh6pm.cmd" -l"libc.a" <Linking> undefined first referenced symbol in file --------- ---------------- SysCtlClockGet ./main.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "PWM_test.out" not built >> Compilation failure gmake: *** [PWM_test.out] Error 1 gmake: Target `all' not remade because of errors. **** Build Finished ****
The same issue also occurs while using the very same code provided by the Workshop.
Can anyone help me?