This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting EK-TM4C1294XL to BOOSTXL-SENSHUB - 5V Pin

Hi there,

I just got by sensor Boosterpack. Before I plug it the other way around and burn something, I wanted to check the pinout diagrams... I plan to use the TM4C129 launchpad.

Well, I measured 5V on pin 2 of either X6 or X8 connectors on the launchpad.

The schematics for the sensor boosterpack seem to expect 3V3 on PIN1 (measured ok), but GND on pin 2, not 5V!

Am I missing something here!?!? Or can I just go ahead and plug that way?

Cheers

Bruno

  • Hi Bruno,

    The SensorHub seamlessly fits on the TM4C129 Connected LaunchPad. To be double-sure, you can mount the Sensor Hub on an unpowered LaunchPad and do a continuity/short check from 5V to GND on the top side of the sensor hub. Similarly between 3.3V & GND and then 5V & 3.3V...

    Does this sound a reasonable method to make sure nothing "burns".

    Regards

    Amit

  • To really insure that, "nothing burns" you must check that no other (unexpected nor unwanted) voltage source feeds into your MCU board!  (certain sensors - or displays - may "boost voltage" and while a, "pro" board should confine/quarantine this voltage - that may not prove universally true.)

    And - simple check for 5V or 3V3 short to ground will not detect the presence of such potentially damaging, foreign voltage.  (note: unlikely does not guarantee non-occurrence!)   (not to ask - how I know!)  Sometimes the best method to "pre-test/verify" an accessory board is to power it while it is "isolated" from all others.  And then systematically probe each/every interconnect pin - looking for unwanted/unexpected voltage levels.  So often you'll find none - but should one/several appear - and were unexpected/improper - you may have prevented a damaging situation.

    I don't know the implementation of your board - but past/similar boards (this vendor) employed the remarkable, deliberate, "pin to pin" shorting of 4 MCU pins.  Should these be set to output - with output levels in conflict - "burn avoidance" may be reduced!