Other Parts Discussed in Thread: EK-TM4C123GXL, TPS2052
Can somebody provide a working project usb host example for ek-tm4c123gxl evalutaion launchpad board with appropriate hardware connection. I couldn't figure it out over days and hours.
//
// Enable all the GPIO peripherals.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
HWREG(GPIO_PORTC_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTC_BASE + GPIO_O_CR) = 0xff;
ROM_GPIOPinConfigure(GPIO_PC6_USB0EPEN);
ROM_GPIOPinTypeUSBDigital(GPIO_PORTC_BASE, GPIO_PIN_6);
ROM_GPIOPinTypeUSBAnalog(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
ROM_GPIOPinTypeUSBAnalog(GPIO_PORTD_BASE, GPIO_PIN_4 | GPIO_PIN_5);
//
// Enable Clocking to the USB controller.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_USB0);
I could not turn the port PB1/USB0VBUS to give 5V I am measuring it with multimeter.
Thanks.