This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB host Controllers and USB hub



Hi,


I am using a TM4c123 series controllers with 1 USB host port. Now I am using the same port using the a USB switch to use the keyboard and pendrive. But i want to use them both without switching. I guess this is possible if a USB HUB controller with 2 or 3 downstream ports is available. So how should go about it, are there any controllers which such capabilities available.

Regards

Dhanush