Other Parts Discussed in Thread: TM4C123GH6PM
Hi, Im using the tm4c123gh6pm launchpad and im trying to set up a connection to my touchscreen controller via SSI. However it seems that I cant even get the SSI to work on its own (no clock pulse or data on SSI0TX when im sending out data from the microcontroller). Since i dont have an oscilloscope at home i am using a multimeter to check the voltage level on the SSI0CLK pin but it does not change levels at all during transmission.
here is my little test code:
#define GPIO_PORTA_DIR_R (*((volatile unsigned long *)0x40004400))
#define GPIO_PORTA_AFSEL_R (*((volatile unsigned long *)0x40004420))
#define GPIO_PORTA_DEN_R (*((volatile unsigned long *)0x4000451C))
#define GPIO_PORTA_AMSEL_R (*((volatile unsigned long *)0x40004528))
#define GPIO_PORTA_PCTL_R (*((volatile unsigned long *)0x4000452C))
#define SSI0_CR0_R (*((volatile unsigned long *)0x40008000))
#define SSI0_CR1_R (*((volatile unsigned long *)0x40008004))
#define SSI0_DR_R (*((volatile unsigned long *)0x40008008))
#define SSI0_SR_R (*((volatile unsigned long *)0x4000800C))
#define SSI0_CPSR_R (*((volatile unsigned long *)0x40008010))
#define SSI0_CC_R (*((volatile unsigned long *)0x40008FC8))
#define SSI_CR0_SCR_M 0x0000FF00 // SSI Serial Clock Rate
#define SSI_CR0_SPH 0x00000080 // SSI Serial Clock Phase
#define SSI_CR0_SPO 0x00000040 // SSI Serial Clock Polarity
#define SSI_CR0_FRF_M 0x00000030 // SSI Frame Format Select
#define SSI_CR0_FRF_MOTO 0x00000000 // Freescale SPI Frame Format
#define SSI_CR0_DSS_M 0x0000000F // SSI Data Size Select
#define SSI_CR0_DSS_8 0x00000007 // 8-bit data
#define SSI_CR1_MS 0x00000004 // SSI Master/Slave Select
#define SSI_CR1_SSE 0x00000002 // SSI Synchronous Serial Port
// Enable
#define SSI_SR_RNE 0x00000004 // SSI Receive FIFO Not Empty
#define SSI_SR_TNF 0x00000002 // SSI Transmit FIFO Not Full
#define SSI_SR_TFE 0x00000001 // SSI Transmit FIFO Empty
#define SSI_CPSR_CPSDVSR_M 0x000000FF // SSI Clock Prescale Divisor
#define SSI_CC_CS_M 0x0000000F // SSI Baud Clock Source
#define SSI_CC_CS_SYSPLL 0x00000000 // Either the system clock (if the
// PLL bypass is in effect) or the
// PLL output (default)
#define SYSCTL_RCGC1_R (*((volatile unsigned long *)0x400FE104))
#define SYSCTL_RCGC2_R (*((volatile unsigned long *)0x400FE108))
#define SYSCTL_RCGC1_SSI0 0x00000010 // SSI0 Clock Gating Control
#define SYSCTL_RCGC2_GPIOA 0x00000001 // port A Clock Gating Control
unsigned int testvalue;
void ssi_Init(void);
unsigned int test(void);
int main(void){
ssi_Init();
while(1){
testvalue = test();
}
}
void ssi_Init(void){
volatile unsigned long delay;
SYSCTL_RCGC1_R |= SYSCTL_RCGC1_SSI0; // activate SSI0
SYSCTL_RCGC2_R |= SYSCTL_RCGC2_GPIOA; // activate port A
delay = SYSCTL_RCGC2_R; // allow time to finish activating
GPIO_PORTA_DIR_R |= 0xC0; // make PA6,7 out
GPIO_PORTA_AFSEL_R |= 0x2C; // enable alt funct on PA2,3,5
GPIO_PORTA_AFSEL_R &= ~0xC0; // disable alt funct on PA6,7
GPIO_PORTA_DEN_R |= 0xEC; // enable digital I/O on PA2,3,5,6,7
// configure PA2,3,5 as SSI
GPIO_PORTA_PCTL_R = (GPIO_PORTA_PCTL_R&0xFF0F00FF)+0x00202200;
// configure PA6,7 as GPIO
GPIO_PORTA_PCTL_R = (GPIO_PORTA_PCTL_R&0x00FFFFFF)+0x00000000;
GPIO_PORTA_AMSEL_R &= ~0xEC; // disable analog functionality on PA2,3,5,6,7
SSI0_CR1_R &= ~SSI_CR1_SSE; // disable SSI
SSI0_CR1_R &= ~SSI_CR1_MS; // master mode
// configure for system clock/PLL baud clock source
SSI0_CC_R = (SSI0_CC_R&~SSI_CC_CS_M)+SSI_CC_CS_SYSPLL;
// clock divider for 2 MHz SSIClk (16 MHz PIOSC/8)
SSI0_CPSR_R = (SSI0_CPSR_R&~SSI_CPSR_CPSDVSR_M)+8;
SSI0_CR0_R &= ~(SSI_CR0_SCR_M | // SCR = 0 (2 Mbps data rate)
SSI_CR0_SPH | // SPH = 0
SSI_CR0_SPO); // SPO = 0
// FRF = Freescale format
SSI0_CR0_R = (SSI0_CR0_R&~SSI_CR0_FRF_M)+SSI_CR0_FRF_MOTO;
// DSS = 8-bit data
SSI0_CR0_R = (SSI0_CR0_R&~SSI_CR0_DSS_M)+SSI_CR0_DSS_8;
SSI0_CR1_R |= SSI_CR1_SSE; // enable SSI
}
unsigned int test(void)
{
volatile unsigned long value = 0;
SSI0_DR_R = 0x90; // data out
while((SSI0_SR_R&10)){}; // wait until data has finished transmitting
value = SSI0_DR_R;
return value;
}