Other Parts Discussed in Thread: TMS570LS1227
Hi,
I am using TMS570LS1227.
I have few doubts on ADC.
1. What I understood from data sheet is, the TMS570 is having only one sampling capacitor for ADC . My doubt is , whether it is one capacitor for both ADC1 & ADC2 or ADC1 and ADC2 has separate sampling capacitors. similarly Group 1 and group2 shares same sampling capacitor or that also having different sampling capacitors.
2. If I configure channel 1 in Group 1 of ADC1 and channel 2 in group2 of ADC1, and both are triggered with same event, how the sampling and conversion will happen.
a) Sampling channel 1 Group1 ADC1 , for time of sample window
b) Group 1 conversion starts and ends conversion
c) discharge of capacitor
d)Channel2 Group 2 ADC1 sampling
e) Group 2 conversion starts
Is my assumption is correct?
3. If there is separate sampling capacitor for each ADC.and I configure ADC1 & ADC2 to sample at same instant, (only one channel is configured in each), Is there any way that I generate interrupt , only when both conversion is complete. or I just use only interrupt from ADC1, and assumed that ADC2 might have completed in same time.?