Other Parts Discussed in Thread: HALCOGEN
http://processors.wiki.ti.com/index.php/HALCoGen_Ethernet_Driver_and_lwIP_Integration_Demonstration
From lwip_main.c, setting static IP should be done accordingly:
/* Initialze the lwIP library, using DHCP.*/
sciDisplayText(sciREGx, txtEnetInit, sizeof(txtEnetInit));
//ipAddr = lwIPInit(0, macAddress, 0, 0, 0, IPADDR_USE_DHCP);
/* Uncomment the following if you'd like to assign a static IP address. Change address as required, and uncomment the previous statement. */
/**/
uint8 ip_addr[4] = { 192, 168, 0, 101 };
uint8 netmask[4] = { 255, 255, 255, 0 };
uint8 gateway[4] = { 192, 168, 0, 1 };
ipAddr = lwIPInit(0, macAddress,
*((uint32_t *)ip_addr),
*((uint32_t *)netmask),
*((uint32_t *)gateway),
IPADDR_USE_STATIC);
This does not work. Any ideas why? (DHCP mode works fine.)