Other Parts Discussed in Thread: TM4C1237H6PZ
hi all,
i am using PART_TM4C1237H6PZ controller, i build code on ccs it is working fine,but when i tried the same code on keil it is not working. I am getting interrupt on USB. my USB configuration is as bellow.
USBStackModeSet(0, eUSBModeForceHost, 0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_USB0);
//
// Configure the required pins for USB operation.
//
GPIOPinConfigure(GPIO_PF4_USB0EPEN); //
GPIOPinConfigure(GPIO_PF5_USB0PFLT); //
GPIOPinTypeUSBAnalog(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1); //id vbs
GPIOPinTypeUSBDigital(GPIO_PORTF_BASE, GPIO_PIN_4 | GPIO_PIN_5); //-
GPIOPinTypeUSBAnalog(GPIO_PORTJ_BASE, GPIO_PIN_0 | GPIO_PIN_1); //dp dm
//
// Configure SysTick for a 100Hz interrupt.
//
SysTickPeriodSet(SysCtlClockGet() / TICKS_PER_SECOND);
SysTickEnable();
SysTickIntEnable();
//
// Enable Interrupts
//
IntMasterEnable();
//
// Initialize the USB stack mode and pass in a mode callback.
//
USBStackModeSet(0, eUSBModeHost, ModeCallback);
//
// Register the host keyboard drivers.
//
USBHCDRegisterDrivers(0, g_ppHostClassDrivers, g_ui32NumHostClassDrivers);
USBHCDInit(0, g_pui8HCDPool, HCD_MEMORY_SIZE);
USBHCDPowerConfigInit(0, USBHCD_VBUS_AUTO_HIGH );
//
// Open an instance of the keyboard driver. The keyboard does not need
// to be present at this time, this just save a place for it and allows
// the applications to be notified when a keyboard is present.
//
g_psKeyboardInstance = USBHKeyboardOpen(KeyboardCallback, g_pui8Buffer, KEYBOARD_MEMORY_SIZE);
Regards,
Dhanush