This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC: Flash on EMIF Byte Enables

Hello,

I'm trying to connect an external 16MiByte asynchronous NOR-Flash to the EMIF-Interface of the TMS570LC. The technical reference manual shows an example interface for connecting a 8MiByte flash to the EMIF (SPNU563 page 826). In this example the byte enable lines are connected to the flash.

The flash chips I wanted to use has no ability to connect byte enables. E.g. http://www.farnell.com/datasheets/1674446.pdf

Is it possible to use a flash without byte enables inputs to the EMIF?

 

Kind regards,

Johannes