Other Parts Discussed in Thread: TMS570LS3137
Hi Folks,
I am working on N2HET of TMS570LS3137.
N2HET instructions are written to detect a rising or falling edge and subsequently raise an HTU request.
If a rising edge is detected then 0x5 is written into a location of the N2HET RAM otherwise for a falling edge 0x7 is written into the same location of the N2HET RAM.
An HTU request is raised subsequently to transfer the Data written in the N2HET RAM to the main memory.
This is working fine. However the HTU transfers the data only once i.e. upon the occurrence of the first event. Any subsequent requests raised by the N2HET is not serviced by the HTU.
The Buffer Full interrupt Flag is being set and HTU is ignoring any new requests from the N2HET.
Can Somebody help me understand why the HTU is getting overloaded with a single request coming from the N2HET.
Regards,
Ru