Hi,
I want to synchronize the RTI & EPWM countuer.
Do you have any good ideas?
Regards,
FSSer
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
We have received your post and will get back to you soon.
Regards.
Hello,
There is one way that you can try and see if it meets your requirements:
You can drive a signal on ePWM1A and this can directly be used by the RTI to clock the free-running counter. No external connection is necessary.
Let me know if this helps.
Regards, Sunil
One caveat with this method: you do need to output the ePWM1A signal onto the pin so that it gets routed back through the I/O cell. This may mean that you lose this pin from being able to connect it to anything else external.
Regards, Sunil