This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137 PBIST Self-check failure / HALCoGen 4.00.00

Hello,

At the end of pbistSelfCheck(), if the self test did not report an error when it should, then notification is called with FAIL1 and the code to restore the state of the PBIST controller is skipped over (restoring PACT and MSTGCR).  Is the restoring skipped for a reason or is this a bug?

Thanks, Charlie Johnston