This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Vinculum VNC1 programming



Hi,

I want to use the FTDI's Vinculum VNc1 controller with two USB host support. I dont know how to program these devices. Wat are the possible solutions. Also is there any firmware for USB HID and Mass storage devices available for these controllers. 

I basically want to develop a device which can be connected to the microcontroller via UART and from the hyperterminal i would be able to send commands to the VNC1 such as file write, read file from usb mass storage device. Is it feasible.

Regards

Sanket