This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137 unable to write to some MibSPI registers right after bringing the SPI out of the reset state



Hi there,

In my code I have the following segment of initialization code for MibSPI1 (similar results for MibSPI3 and MibSPI5):

void tagMibSpi1::InitSpi()                  // initialize SPI device
{
    // general MibSPI control registers initialization ------------------------

    MIBSPI1GCR0     = 0x00000001;           // bring this SPI out of reset state
    MIBSPI1MIBSPIE  = 0x00000001;           // enable multi-buffer mode

    MIBSPI1PC0      = 0x00000E17;           // set appropriate pins to SPI functions
    MIBSPI1DEF      = 0x000000FF;           // set default chip-selects
    MIBSPI1FMT0     = 0x00010510;           // set phase, data format 0 and timestamp
    MIBSPI1UERRCTRL = 0x0000000A;           // enable parity error detection


    // transfer group 0 configuration -----------------------------------------
    //
    // Note: By setting the TRIGSRC to 0 (none), the TRIGEVT to 7h (always), and the
    //       ONESHOT bit to 1, software can trigger this TG. Upon setting the
    //       TGENA bit, the TG is immediately triggered. If ONESHOTx is set
    //       the transfer is performed only once.

    MIBSPI1TG0CTRL_bit.ONESHOT = 1;         // only once (need to re-enable TGENA bit after transfer)
    MIBSPI1TG0CTRL_bit.TRIGEVT = 0x7;       // always (for SW trigger, see note above)
    MIBSPI1TG0CTRL_bit.TRIGSRC = 0x0;       // disable trigger source (SW trigger)
    MIBSPI1TG0CTRL_bit.PSTART  = MIBSPI1_TG0_EL_START;

    ...

}

With the above code, I have observed that the MIBSPI1UERRCTRL and MIBSPI1TG0CTRL registers were unmodified as intended after execution of the above code. If I put a breakpoint at the line MIBSPI1GCR0= then continue, nothing changes; but if I put a breakpoint at the line MIBSPI1MIBSPIE= then continue, all is fine.

Then I see the "Auto Initialization of Multibuffer RAM" starting after bringing the SPI out of the reset state ... with the MIBSPIxGCR0=1.

My question is: what is the delay to wait after bringing the SPI out of the reset state? What register should I poll before going ahead to configure the SPI?

Thanks.