Hello,
I am Using BOSTXL-SENSHUB Board with TIVA C-series launchpad evaluation kit. I am trying to use this for compass application, but getting some Trouble with it,
The Sensor Used is MPU-9150.
I am interpreting the calculated "YAW" for finding the Direction with respect to north.
The problem is, It shows a non-linear scale.
The north is shifted by 20° right from actual north.
The West which the board is showing is at 65° Right form actual north,
South is at 160° Right From actual north ,
and east is indicated at 70 ° left from Actual north.
Can anyone help me on this.
I am not understanding the problem whether I am interpreting it wrong ar it is a problem of sensor IC.
Thanks
Akshay Joshi