This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pwm module

i want to output a pwm pulse, its duty cycle is varied according to addition of the two pwm pulse generated according to the sinusoidal pwm technique.

  • Hello Archu,

    We need to know some more information

    1. What is the TIVA Device you are targetting it for

    2. Is there a response time requirement from the addition of the two input pwm pulses to output of the pwm pulse. Please note that TM4C devices do not have a arithmetic block to do it on the fly and would need CPU intervention so a delay in response would be expected.

    Regards

    Amit

  • hi,

    thank you for your response.

    i am currently using tm4c123g.


    my current problem is that i want to generate a pwm signal with its duty cycle continuously changing.(changes according to the signal generated by adding two sinusoidal pwm signals). how can i implement this?.can i use the GPIO output as pwm signal?.

    Regards

    Archu

     

  • Your description of your requirement (appears) to spectacularly exceed your time/effort in MCU manual read/review...

    Few sentences into the gpio section of that manual will answer your gpio output as pwm question.  (No)

    A large chapter - greatly detailing PWM set-up & operation - awaits those willing to do, (some) work...