Other Parts Discussed in Thread: EK-TM4C123GXL
Since I've had excellent support from the forum in the past I thought I would try again. Kind thanks, all.
I am working with the above launchpad board initially and am trying to set up two sequencers to do identical work however I want to use the second ADC (ie ADC1) to convert the last pair of four channels. I realise on the Launchpad board, ADC Ch3 is not brought out to a pin but that's not important to me in developing code.
// Enable the ADCs internally
SysCtlPeripheralEnable( SYSCTL_PERIPH_ADC0 );
SysCtlPeripheralEnable( SYSCTL_PERIPH_ADC1 );
#ifdef LAUNCHPAD
//Enable Pin inputs
SysCtlPeripheralEnable( SYSCTL_PERIPH_GPIOE );
GPIOPinTypeADC( GPIO_PORTE_BASE, GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0 );
#else
// for our board
#endif
// Enable the first sample sequencer to capture the value of channel 0 when
// the processor trigger occurs.
ADCSequenceDisable( ADC0_BASE, SEQ1 );
ADCSequenceConfigure( ADC0_BASE, SEQ1, ADC_TRIGGER_ALWAYS, PRIORITY1 );
ADCSequenceStepConfigure( ADC0_BASE, SEQ1, STEP0, ADC_CTL_CH0 );
ADCSequenceStepConfigure( ADC0_BASE, SEQ1, STEP1, ADC_CTL_CH1 | ADC_CTL_IE | ADC_CTL_END );
// And do the same for the second sequencer
ADCSequenceDisable( ADC1_BASE, SEQ2 );
ADCSequenceConfigure( ADC1_BASE, SEQ2, ADC_TRIGGER_ALWAYS, PRIORITY0 );
ADCSequenceStepConfigure( ADC1_BASE, SEQ2, STEP0, ADC_CTL_CH2 );
ADCSequenceStepConfigure( ADC1_BASE, SEQ2, STEP1, ADC_CTL_CH3 | ADC_CTL_IE | ADC_CTL_END );
//setup interrupts
ADCIntRegister(ADC0_BASE, SEQ1, ADCinterruptSequencer1);
ADCIntRegister(ADC1_BASE, SEQ2, ADCinterruptSequencer2);
ADCIntClear(ADC0_BASE, SEQ1);
ADCIntClear(ADC1_BASE, SEQ2);
ADCIntEnable(ADC0_BASE, SEQ1);
ADCIntEnable(ADC1_BASE, SEQ2);
}
What I have done is a complete carbon copy of the working code seen above for ADC0. However, the interrupt is never called (ie the interrupt routine is never entered, so I have not bothered to include it here).
Perhaps someone has some initial thoughts where I may be going wrong or if ADC1 requires special configuration that ADC0 does not.
Thanks in advance