Other Parts Discussed in Thread: EK-TM4C123GXL
Greetings, once again, i come up with a possible solution for the communication between 2 TM4C123GXL launchboard, bu for now i haven't been able to make routines execute. I suppose its because im using a Timer interrupt to execute a button interrupt, so the interrups are somehow causing troubles i guess.
My master have this code:
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_gpio.h"
#include "inc/hw_ints.h"
#include "inc/hw_nvic.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/pwm.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "driverlib/buttons.h"
#include "driverlib/adc.h"
#include "driverlib/timer.h"
#include "math.h"
#include "driverlib/ssi.h"
//*****************************************************************************
#define NUM_SSI_DATA 10
volatile unsigned long g_ulSSI2RXTO = 0;
uint32_t g_DataRx2[NUM_SSI_DATA];
uint32_t g_DataTx2[NUM_SSI_DATA];
uint32_t ulDataRx2[NUM_SSI_DATA];
uint32_t ulDataTx2[NUM_SSI_DATA];
unsigned long ulStatus, g_Index, ulPeriod, ulindex;
int mode;
extern void IntGPIOB(void);
void Timer1IntHandler(void);
void Init (void){
ROM_SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
// Desbloquear portas F do NMI
/*HWREG (GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG (GPIO_PORTF_BASE + GPIO_O_CR) |= GPIO_PIN_0;
HWREG (GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_M;*/
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1 | GPIO_PIN_2 |GPIO_PIN_3);
}
void InitUart (void) {
// UART Initialization
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioConfig(0, 115200, 80000000);
}
void InitTimer (void) {
ulPeriod = (ROM_SysCtlClockGet()/100) ;
ROM_TimerConfigure(TIMER1_BASE, TIMER_CFG_PERIODIC);
ROM_TimerLoadSet(TIMER1_BASE, TIMER_A, ulPeriod -1);
// Enable interruption Timer 1
IntEnable(INT_TIMER1A);
ROM_TimerIntEnable(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
ROM_TimerEnable(TIMER1_BASE, TIMER_A);
ROM_IntMasterEnable();
}
void InitButtonInt (void){
GPIOPinTypeGPIOInput(GPIO_PORTB_BASE, GPIO_PIN_5);
GPIOPadConfigSet(GPIO_PORTB_BASE,GPIO_PIN_5,GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD_WPU);
GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_5,GPIO_PIN_5);
GPIOIntDisable(GPIO_PORTB_BASE, GPIO_INT_PIN_5);
GPIOIntTypeSet(GPIO_PORTB_BASE, GPIO_PIN_5, GPIO_FALLING_EDGE);
GPIOIntClear(GPIO_PORTB_BASE, GPIO_INT_PIN_5);
GPIOIntRegister(GPIO_PORTB_BASE,IntGPIOB);
GPIOIntEnable(GPIO_PORTB_BASE, GPIO_PIN_5);
ROM_IntMasterEnable();
}
void InitSPI2(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);
GPIOPinConfigure(GPIO_PB4_SSI2CLK);
//GPIOPinConfigure(GPIO_PB5_SSI2FSS);
GPIOPinConfigure(GPIO_PB6_SSI2RX);
GPIOPinConfigure(GPIO_PB7_SSI2TX);
GPIOPinTypeSSI(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_6 | GPIO_PIN_7);
SSIConfigSetExpClk(SSI2_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_3, SSI_MODE_MASTER, 115200, 10);
SSIEnable(SSI2_BASE);
}
int main(void)
{
//volatile int ulLoop;
Init();
InitUart();
InitButtonInt();
InitTimer();
InitSPI2();
while(1)
{
//_____________________Main Cycle___________________________
}
}
void IntGPIOB(void)
{
GPIOIntClear(GPIO_PORTB_BASE, GPIO_PIN_5);
UARTprintf("IF MODE\n ");
if (mode==0){
ulDataTx2[0] = 100;
ulDataTx2[1] = 200;
ulDataTx2[2] = 300;
ulDataTx2[3] = 400;
ulDataTx2[4] = 500;
ulDataTx2[5] = 600;
ulDataTx2[6] = 700;
ulDataTx2[7] = 800;
ulDataTx2[8] = 900;
ulDataTx2[9] = 1000;
while(SSIDataPutNonBlocking(SSI2_BASE, ulDataTx2[0]))
{
UARTprintf("SSIDataPutNonBlocking\n ");
}
UARTprintf("Enviado:\n ");
for(ulindex = 0; ulindex < NUM_SSI_DATA; ulindex++)
{
SSIDataPut(SSI2_BASE, ulDataTx2[ulindex]);
UARTprintf("%4d ", ulDataTx2[ulindex]);
}
while(SSIBusy(SSI2_BASE))
{
}
mode++;
GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_5,GPIO_PIN_5);
}
else {
UARTprintf("Recebido:\n ");
for(ulindex = 0; ulindex < NUM_SSI_DATA; ulindex++)
{
SSIDataGet(SSI2_BASE, &ulDataRx2[ulindex]);
UARTprintf("%4d ", ulDataRx2[ulindex]);
}
while(SSIBusy(SSI2_BASE))
{
}
mode=0;
GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_5,GPIO_PIN_5);
}
}
//count++;
//UARTprintf("Count = %4d \n", count);
void Timer0IntHandler(void)
{
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
}
void Timer1IntHandler(void)
{
GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_5,0);
//rpm=count*60/cog;
//count=0;
//UARTprintf("Timerinterrupt = %4d \n", count);
TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
}
I think its quite clear what im trying to do. I have checked the startup code also, and everything is in order.Somehow the timer1 its now executing but doesn't trigger the button interrupt, not detecting the FALLING_EDGE. Can you guys come up with a solution?