This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VDDC Pin connection on TM4C1231H6PM

Other Parts Discussed in Thread: TM4C1231H6PM

Hello friends,

i am wondering about the right connection of the VDDC pins 25 and 56 of my TM4C1231H6PM.

The datasheet says:

Positive supply for most of the logic function, including the processor core and most peripherals. The voltage on this pin is 1.2 V and is supplied by the on-chip LDO. The VDDC pins should only be connected to each other and an external capacitor as specified in Table 21-12 on page 1111 .

But do i have to connect pins 25 and 56 with each other?

I have designed the VDDC capacitor in accordance with the TM4C123GXL LaunchPad, having 100nF on both pins, 1µF on pin 25 and 2.2µF on pin 56. Also, i have both pins connected, but if it is possible, i would like not to connect them.

Cheers

Janos