This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DK-TM4C129X UART start bit

Other Parts Discussed in Thread: TM4C129XNCZAD

Hello,

recently ported an application to DK-TM4C129X which contains the TM4C129XNCZAD. I noticed some problems in serial communication with a device hooked up to the RX/TX on the board. The device would not respond as I would expect it to do (it only responds to a single command, so I decided to debug the TX line towards the device).


My UART settings are:

- 9600bps

- 8 data bits

- 1 stop bit

- no parity

To debug the TX output I contiuously output 0xAD (10101101). Attached image is the result on my scope. As can be seen the start bit is a '1'. Shouldn't this be a '0'?