I'm having trouble importing and running example projects from TivaWare. With many of the projects for the TM4C123G I was able to figure out the necessary missing files to get some of the projects to build but I'm having more trouble with the TM4C129X examples.
With the simple blinky project I am able to import, build and run the code.
Trying to get the sd_card example working is another story.
File -> Import... -> CCS Project -> ../MyTivaWareInstallationDir/examples/boards/dk-tm4c129x/sd_card
Build. Produces errors
[Console Output] **** Build of configuration Debug for project sd_card **** /home/jamie/ti/ccsv6/utils/bin/gmake -k all Building file: ../sd_card.c Invoking: ARM Compiler "/home/jamie/ti/ccsv6/tools/compiler/arm_5.1.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -O2 -g --include_path="/home/jamie/ti/ccsv6/tools/compiler/arm_5.1.6/include" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573/examples/boards/dk-tm4c129x" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573/third_party" --gcc --define=ccs="ccs" --define=PART_TM4C129XNCZAD --define=TARGET_IS_TM4C129_RA0 --define=ENABLE_LFN --define=UART_BUFFERED --diag_warning=225 --display_error_number --diag_wrap=off --gen_func_subsections=on --ual --preproc_with_compile --preproc_dependency="sd_card.pp" "../sd_card.c" Finished building: ../sd_card.c Building file: ../startup_ccs.c Invoking: ARM Compiler "/home/jamie/ti/ccsv6/tools/compiler/arm_5.1.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -O2 -g --include_path="/home/jamie/ti/ccsv6/tools/compiler/arm_5.1.6/include" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573/examples/boards/dk-tm4c129x" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573/third_party" --gcc --define=ccs="ccs" --define=PART_TM4C129XNCZAD --define=TARGET_IS_TM4C129_RA0 --define=ENABLE_LFN --define=UART_BUFFERED --diag_warning=225 --display_error_number --diag_wrap=off --gen_func_subsections=on --ual --preproc_with_compile --preproc_dependency="startup_ccs.pp" "../startup_ccs.c" Finished building: ../startup_ccs.c Building target: sd_card.out Invoking: ARM Linker "/home/jamie/ti/ccsv6/tools/compiler/arm_5.1.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -O2 -g --gcc --define=ccs="ccs" --define=PART_TM4C129XNCZAD --define=TARGET_IS_TM4C129_RA0 --define=ENABLE_LFN --define=UART_BUFFERED --diag_warning=225 --display_error_number --diag_wrap=off --gen_func_subsections=on --ual -z --stack_size=1024 -m"sd_card_ccs.map" --heap_size=0 -i"/home/jamie/ti/ccsv6/tools/compiler/arm_5.1.6/lib" -i"/home/jamie/ti/ccsv6/tools/compiler/arm_5.1.6/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="sd_card_linkInfo.xml" --rom_model -o "sd_card.out" "./startup_ccs.obj" "./sd_card.obj" "../sd_card_ccs.cmd" -l"libc.a" -l"/home/jamie/ti/TivaWare_C_Series-2.1.0.12573/examples/boards/dk-tm4c129x/sd_card/ccs/../../../../../driverlib/ccs/Debug/driverlib.lib" -l"/home/jamie/ti/TivaWare_C_Series-2.1.0.12573/examples/boards/dk-tm4c129x/sd_card/ccs/../../../../../grlib/ccs/Debug/grlib.lib" <Linking> warning #10229-D: output section ".data" refers to load symbol "g_sKentec320x240x16_SSD2119" and hence cannot be compressed; compression "rle" is ignored undefined first referenced symbol in file --------- ---------------- CmdLineProcess ./sd_card.obj FrameDraw ./sd_card.obj Kentec320x240x16_SSD2119Init ./sd_card.obj PinoutSet ./sd_card.obj TouchScreenCallbackSet ./sd_card.obj TouchScreenInit ./sd_card.obj TouchScreenIntHandler ./startup_ccs.obj UARTPeek ./sd_card.obj UARTStdioConfig ./sd_card.obj UARTStdioIntHandler ./startup_ccs.obj UARTgets ./sd_card.obj UARTprintf ./sd_card.obj disk_timerproc ./sd_card.obj f_mount ./sd_card.obj f_opendir ./sd_card.obj f_readdir ./sd_card.obj g_sKentec320x240x16_SSD2119 ./sd_card.obj usnprintf ./sd_card.obj uvsnprintf ./sd_card.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "sd_card.out" not built >> Compilation failure gmake: *** [sd_card.out] Error 1 gmake: Target `all' not remade because of errors. **** Build Finished ****
Project Properties
Include paths. Properties -> CCS Build -> ARM Compiler -> Inlcude Options [Add dir to #include...]
"${CG_TOOL_ROOT}/include"
"${SW_ROOT}/examples/boards/dk-tm4c129x"
"${SW_ROOT}"
"${SW_ROOT}/third_party"
Build variables. Properties -> C/C++ Build -> Build Variables
ORIGINAL_PROJECT_ROOT Directory /home/jamie/ti/TivaWare_C_Series-2.1.0.12573/examples/boards/dk-tm4c129x/sd_card/ccs
SW_ROOT Directory ${ORIGINAL_PROJECT_ROOT}/../../../../..
Compiler Flags. Properties -> CCS Build -> ARM Compiler
-mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -O2 -g --include_path="/home/jamie/ti/ccsv6/tools/compiler/arm_5.1.6/include" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573/examples/boards/dk-tm4c129x" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573" --include_path="/home/jamie/ti/TivaWare_C_Series-2.1.0.12573/third_party" --gcc --define=ccs="ccs" --define=PART_TM4C129XNCZAD --define=TARGET_IS_TM4C129_RA0 --define=ENABLE_LFN --define=UART_BUFFERED --diag_warning=225 --display_error_number --diag_wrap=off --gen_func_subsections=on --ual
Library files. Properties -> CCS Build -> ARM Linker -> File Search Path
[include library file or command file..]
"libc.a"
"${SW_ROOT}/driverlib/ccs/Debug/driverlib.lib"
"${SW_ROOT}/grlib/ccs/Debug/grlib.lib"
[Add <dir> to library search path..]
"${CG_TOOL_ROOT}/lib"
"${CG_TOOL_ROOT}/include"
Directory Listings.
[project folder]
~/ccs/sd_card/
.ccsproject
.cproject
Debug/
macros.ini_initial
.project
sd_card.c
sd_card_ccs.cmd
.settings/
startup_ccs.c
target_config.ccxml
[sd_card example project folder]
~/ti/TivaWare_C_Series-2.1.0.12573/examples/boards/dk-tm4c129x/sd_card/
ccs/
.ccsimportspec
.ccsproject
.cproject
Debug/
macros.ini_initial
.project
.settings/
target_config.ccxml
ewarm/
gcc/
Makefile
readme.txt
rvmdk/
sd_card.c
sd_card_ccs.cmd
sd_card.ewd
sd_card.ewp
sd_card.icf
sd_card.ld
sd_card.sct
sd_card.uvopt
sd_card.uvproj
startup_ccs.c
startup_ewarm.c
startup_gcc.c
startup_rvmdk.S
I also tried importing qs_weather but even after following this thread http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/337769/1178701.aspx#1178701 I wasn't able to get it to build.
I'm assuming there is an issue with linked/missing files. I have experimented with adding several more include paths as well as directly adding files like "utils/uartstdio.c" to my project folder. All sorts of include paths added for directories under third_party. I was able to get passed some of the unresolved symbols this way but continued to hit walls.
Can anyone spot the issue? I expected problems after going through similar issues with the TM4C123G example projects but these missing dependencies are maddening.