This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ROM_SysCtlDelay declared implicitly/unresolved symbol



I decided I would modify the blinky project (dk-tm4c129x) because I'll likely want to make some LED error codes in the future. Blinky uses the LEDs differently than I am used to, avoiding calls to ROM_SysCtlPeripheralEnable, ROM_GPIOPinTypeGPIOOutput, GPIOPinWrite and ROM_SysCtlDelay.

I decided as practice I would try to transform blinky to use these as opposed to writing directly as it was.

Unfortunately I've been held up immediately and I can't figure out why I'm getting this unresolved symbol error.

My first change was to replace the for loops with ROM_SysCtlDelay's.

#include <stdint.h>
#include "driverlib/rom.h"
#include "inc/tm4c129xnczad.h"

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Blinky (blinky)</h1>
//!
//! A very simple example that blinks the on-board LED.
//
//*****************************************************************************

//*****************************************************************************
//
// Blink the on-board LED.
//
//*****************************************************************************
int
main(void)
{
    volatile uint32_t ui32Loop;

    //
    // Enable the GPIO port that is used for the on-board LED.
    //
    SYSCTL_RCGCGPIO_R = SYSCTL_RCGCGPIO_R14;

    //
    // Do a dummy read to insert a few cycles after enabling the peripheral.
    //
    ui32Loop = SYSCTL_RCGCGPIO_R;

    //
    // Enable the GPIO pin for the LED (PQ7).  Set the direction as output, and
    // enable the GPIO pin for digital function.
    //
    GPIO_PORTQ_DIR_R = 0x80;
    GPIO_PORTQ_DEN_R = 0x80;

    //
    // Loop forever.
    //
    while(1)
    {
        //
        // Turn on the LED.
        //
        GPIO_PORTQ_DATA_R |= 0x80;

        //
        // Delay for a bit.
        //
        //for(ui32Loop = 0; ui32Loop < 200000; ui32Loop++)
       // {
       // }
        ROM_SysCtlDelay(200000);

        //
        // Turn off the LED.
        //
        GPIO_PORTQ_DATA_R &= ~(0x80);

        //
        // Delay for a bit.
        //
        for(ui32Loop = 0; ui32Loop < 200000; ui32Loop++)
        {
        }
    }
}

If I click f3 on "driverlib/rom.h" it takes me to the header, searching the header I'm able to find ROM_SysCtlDelay which should be defined if TARGET_IS_TM4C129_RA1 (which is defined in my compile time flags)

This one just doesn't make any sense to me. Any ideas?