Other Parts Discussed in Thread: TM4C1292NCPDT, TM4C129CNCPDT
Hello,
I'm getting a Tivaware assert when I call the following 2 functions on a TM4C1292NCPDT.
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER6);
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER7);
The assert that fails is:
ASSERT(_SysCtlPeripheralValid(ui32Peripheral));
Which is understandable since this function does not have an entry for Timer 6 or Timer 7.
The data sheet says that it has 8 timer modules and the part header file has entries for 6 and 7, however, Tivaware and the PinMux utility do not seem to support enabling it.
Is that because these 2 timers are not mapped to any external CCP module?
Thanks,
Dominic