Hi, I am developing for the RM48l950PGE and looking at the self tests. I have found a couple of issues here. We primarily use version 3.8.01, but I updated to 4.0.0 and found the same issues.
When I enable Flash ECC Check, it adds a call to _coreEnableFlashEcc_() in sys_startup.c, but when I remove the check from the check box and regenerate, the function does not go away.
When I check EMAC SP RAM under Memory Built In Self test Enable, it causes a syntax error from a misconstructed block comment.
Can anyone tell me if these are being fixed?
Thanks,
Westin