This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

functions timer capture time and match set are compatible?

Hey guys!

I'm trying synchronize both Timer functions - capture time and match set timeout that work both, but im only get timer event capture interrupt.. I'm checking it by TimerIntStatus get value..

What I want to do, is get interrupt then changes Pin status (get edge changed) and then timer time is timeout.. (this case 30 000 ticks) It is possible?

#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"

int Edge[400];
int Buffer_lenght = 0;
uint32_t z = 0;

void Timer2BIntHandler(void)
{
    z = TimerIntStatus(TIMER2_BASE, 1);

    TimerIntClear(TIMER2_BASE, z);

    Edge[Buffer_lenght] = TimerValueGet(TIMER2_BASE, TIMER_B);
    Buffer_lenght++;
}

int main(void)
{
    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_INT);

    SysCtlDeepSleepClockSet(SYSCTL_DSLP_PIOSC_PD);
    SysCtlPeripheralClockGating(true);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER2);
    SysCtlPeripheralDeepSleepEnable(SYSCTL_PERIPH_TIMER2);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);

    GPIOPinConfigure(GPIO_PB1_T2CCP1);

    GPIOPinTypeTimer(GPIO_PORTB_BASE, GPIO_PIN_1);

    TimerConfigure(TIMER2_BASE, TIMER_CFG_SPLIT_PAIR | TIMER_CFG_B_CAP_TIME_UP);

    TimerControlEvent(TIMER2_BASE, TIMER_B, TIMER_EVENT_BOTH_EDGES);

    TimerPrescaleSet(TIMER2_BASE, TIMER_B, 16);
    
    TimerMatchSet(TIMER2_BASE, TIMER_B, 30000);

    IntEnable(INT_TIMER2B);

    TimerIntEnable(TIMER2_BASE, TIMER_CAPB_EVENT | TIMER_CAPB_MATCH);

    IntMasterEnable();

    TimerEnable(TIMER2_BASE, TIMER_B);

    while(1)
    {
        SysCtlDeepSleep();
    }
}