Hello everyone,
I need to protect code from unautorized readings. Is there any way to do that? or somthing similar?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
I need to protect code from unautorized readings. Is there any way to do that? or somthing similar?
Thanks
Hi, there.
Would you please provide the part number of the TMS470 device you are using?
Thanks and regards,
Zhaohong
Raul,
There is no such feature on this device.
Thanks and regards,
Zhaohong
Raul,
We would suggest upgrading to a product like http://www.ti.com/product/tms570ls0432
This has very similar peripherals and system as the TMS470MF06607 both are based on the same platform architecture. This product has an IP called AJSM that allows you to lock the debug port and prevent unauthorized read of flash. You can unlock it with a key that you burn yourself into the OTP so you'll still be able to debug but others can't snoop.