This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with use Uart2 using TM4c123g

Hello, i'm student from Brazil. And i tryed to use uart2 to having comunication to my hc-05 bluetooth module. But i don't know how unlock the pin( PD7, PD6) for that. I read all the forum and nothing resolves. Every time give me the same result. Every time, when program do the line "GPIOPinConfigure(GPIO_PCTL_PD7_U2TX);" result in FaultISR.

All my code is below.

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"


#include "driverlib/gpio.c"
#include "driverlib/pin_map.h"
#include "inc/lm4f120h5qr.h"



//#include "inc/hw_memmap.h"
//#include "inc/hw_types.h"
//#include "driverlib/gpio.h"
//#include "driverlib/pin_map.h"
//#include "driverlib/sysctl.h"
//#include "driverlib/uart.h"
//#include "inc/lm4f120h5qr.h"

int main(void) {
	
	SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);

	SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);   //habilita a porta B

	//HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
	//HWREG(GPIO_PORTD_BASE + GPIO_O_CR) = 0x80;

   // HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) =  0x4C4F434B;   //GPIO_LOCK_KEY; 0x4C4F434B// 0xACCE551
   // HWREG(GPIO_PORTD_BASE + GPIO_O_CR) |= 0xC0;
   // HWREG(GPIO_PORTD_BASE + GPIO_O_AFSEL) &= ~0x80;
  //  HWREG(GPIO_PORTD_BASE + GPIO_O_DEN) |= 0x80;
   // HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = 0;


    // Unlock access to the commit register
    HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;

    //
    // Set the commit register for PD7 to allow changing the function
    //
    HWREG(GPIO_PORTD_BASE + GPIO_O_CR) = 0x80;

    //
    // Enable the alternate function for PD7 (U2TX)
    //
    HWREG(GPIO_PORTD_BASE + GPIO_O_AFSEL) |= 0x400;

    //
    // Turn on the digital enable for PD7
    //
    HWREG(GPIO_PORTD_BASE + GPIO_O_DEN) |= 0x80;

    //
    // Relock the commit register
    //
    HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = 0;

    GPIOPinConfigure(GPIO_PCTL_PD7_U2TX);    //quer disser que o pino pb7 vai ser o TX

    SysCtlDelay(20000000);

    GPIOPinConfigure(GPIO_PCTL_PD6_U2RX);    //quer disser que o pino pb6 vai ser o RX

    SysCtlPeripheralEnable(SYSCTL_PERIPH_UART2);   //vai habilitar o modulo 1 uart2


  //  GPIO_PCTL_PB0_U1RX
  //  GPIOPinConfigure(GPIO_PA0_U0RX);
   // GPIOPinConfigure(GPIO_PA1_U0TX);

    //GPIOPinConfigure(GPIO_PCTL_PA0_U0RX);
   // GPIOPinConfigure(GPIO_PCTL_PA1_U0TX);




    GPIOPinTypeUART(GPIO_PORTD_BASE, GPIO_PIN_7 | GPIO_PIN_6); //vai setar as portas como uart



    //na prototipação é qual uart vai ser, o valor do clock, baud rate, numerodebits|1bitdeparada|sembitdeparidade

    UARTConfigSetExpClk(UART2_BASE, SysCtlClockGet(), 9600,
    		(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));  //com4

    UARTCharPut(UART2_BASE, 'E');
    UARTCharPut(UART2_BASE, 'n');
    UARTCharPut(UART2_BASE, 't');
    UARTCharPut(UART2_BASE, 'e');
    UARTCharPut(UART2_BASE, 'r');
    UARTCharPut(UART2_BASE, ' ');
    UARTCharPut(UART2_BASE, 'T');
    UARTCharPut(UART2_BASE, 'e');
    UARTCharPut(UART2_BASE, 'x');
    UARTCharPut(UART2_BASE, 't');
    UARTCharPut(UART2_BASE, ':');
    UARTCharPut(UART2_BASE, ' ');

    while (1)
    {
        UARTCharPut(UART2_BASE, '1');
        UARTCharPut(UART2_BASE, '2');
        UARTCharPut(UART2_BASE, '3');
        UARTCharPut(UART2_BASE, '4');
        UARTCharPut(UART2_BASE, '5');
        UARTCharPut(UART2_BASE, '6');
        UARTCharPut(UART2_BASE, ' ');
        SysCtlDelay(20000000);
    	//if (UARTCharsAvail(UART0_BASE)) UARTCharPut(UART0_BASE, UARTCharGet(UART0_BASE));
    }

}

  • Just do this:

    HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
    HWREG(GPIO_PORTD_BASE + GPIO_O_CR) = 0x80;
    you can see in table in datasheet page 617, that PD[7] and  PF[0] are indeed locked and that you need to work with the GPIOLOCK register and the GPIOCR (page 684 and 685 if your interested in seing that)
  • Hello All,

    Please replace the following code (there are some issues in the code you have like AFSEL moved into the wrong position)

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);   //habilita a porta B
    
    //HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
    //HWREG(GPIO_PORTD_BASE + GPIO_O_CR) = 0x80;
    
    // HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) =  0x4C4F434B;   //GPIO_LOCK_KEY; 0x4C4F434B// 0xACCE551
    // HWREG(GPIO_PORTD_BASE + GPIO_O_CR) |= 0xC0;
    // HWREG(GPIO_PORTD_BASE + GPIO_O_AFSEL) &= ~0x80;
    //  HWREG(GPIO_PORTD_BASE + GPIO_O_DEN) |= 0x80;
    // HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = 0;
    
    
        // Unlock access to the commit register
        HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
    
        //
        // Set the commit register for PD7 to allow changing the function
        //
        HWREG(GPIO_PORTD_BASE + GPIO_O_CR) = 0x80;
    
        //
        // Enable the alternate function for PD7 (U2TX)
        //
        HWREG(GPIO_PORTD_BASE + GPIO_O_AFSEL) |= 0x400;
    
        //
        // Turn on the digital enable for PD7
        //
        HWREG(GPIO_PORTD_BASE + GPIO_O_DEN) |= 0x80;
    
        //
        // Relock the commit register
        //
        HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = 0;
    
        GPIOPinConfigure(GPIO_PCTL_PD7_U2TX);    //quer disser que o pino pb7 vai ser o TX
    
        SysCtlDelay(20000000);
    
        GPIOPinConfigure(GPIO_PCTL_PD6_U2RX);    //quer disser que o pino pb6 vai ser o RX

    with

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD); //habilita a porta B

    SysCtlDelay(10);

    // Unlock access to the commit register
        HWREG(GPIO_PORTD_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
    
        //
        // Set the commit register for PD7 to allow changing the function
        //
        HWREG(GPIO_PORTD_BASE + GPIO_O_CR) |= 0x80;

    GPIOPinType(GPIO_PD6_U2RX);
    GPIOPinType(GPIO_PD7_U2TX);
    GPIOPinTypeUART(GPIO_PORTD_BASE, GPIO_PIN_7 | GPIO_PIN_6);

    Regards

    Amit