We use TMS570LS20216 in one of our design, where we intent to drive the processor with the 20MHz external clock input as it supports from 5MHz to 20MHz per the datasheet. However I am curious whether the tolerance (ppm) of any type of 20MHz oscillator that may drive a little additional than the 20MHz (say 20.002MHz if I use 100 PPM oscillator device, for an example) will be a problem? In that case if I consider the datasheet I can’t use any of the 20MHz oscillator right? Can you please help me to know whether any additional increase on the upper limits to account any practical 20MHz external oscillator with a definite stability / tolerance on frequency.
Thanks & Best Regards,
Jawahar