I'm facing an interesting problem. I want to interface my Connected Launchpad with TM4C1294 with an external gateway device, which sends different amount of data different time. I have connected device to UART5 and and tried to echo what I receive at UART5 to UART0 and vice versa. If I'm using a while loop inside my main function for that, I'm getting everything working. The code is like this.
int main( void ) {
// configure board and peripherals
// .......
// infinite loop
while (1) {
while( UARTCharsAvail(UART0_BASE) ) {
UARTCharPut( UART5_BASE, UARTCharGet( UART0_BASE ) );
}
while( UARTCharsAvail(UART5_BASE) ) {
UARTCharPut( UART0_BASE, UARTCharGet( UART5_BASE ) );
}
} // end of main
But If I write the same code with interrupts I'm experiencing data loss. Here is my full code :
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
uint32_t g_ui32SysClock;
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
void UARTIntHandler_device(void)
{
uint32_t ui32Status;
uint8_t i = 0, j = 0;
uint8_t recvBuffer[100];
IntDisable( INT_UART0 );
IntDisable( INT_UART5 );
ui32Status = UARTIntStatus(UART5_BASE, true);
UARTIntClear(UART5_BASE, ui32Status);
while(UARTCharsAvail(UART5_BASE)) {
if( i < 100 ) {
recvBuffer[i] = UARTCharGet(UART5_BASE);
i++;
}
// Blink the LED to show a character transfer is occuring.
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
SysCtlDelay(g_ui32SysClock / (1000 * 3)); // Delay for 1ms.
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
}
// Send it to PC
for( j = 0; j < i; j++ ) {
UARTCharPut( UART0_BASE, recvBuffer[j] );
}
IntEnable( INT_UART0 );
IntEnable( INT_UART5 );
}
void UARTIntHandler_PC( void ) {
uint32_t ui32Status;
char data = 0;
IntMasterDisable();
ui32Status = UARTIntStatus(UART0_BASE, true);
UARTIntClear(UART0_BASE, ui32Status);
while( UARTCharsAvail(UART0_BASE) ) {
data = UARTCharGetNonBlocking( UART0_BASE );
// UARTCharPut( UART0_BASE, data );
UARTCharPut( UART5_BASE, data );
}
IntMasterEnable();
}
int main(void)
{
g_ui32SysClock = MAP_SysCtlClockFreqSet( ( SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480 ),
120000000 );
// Set up LEDs
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
// Setup UART0 for connection to PC
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTConfigSetExpClk(UART0_BASE, g_ui32SysClock, 57600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
// Setup UART5 for connection to EnOcean Pi
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART5);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
GPIOPinConfigure(GPIO_PC6_U5RX);
GPIOPinConfigure(GPIO_PC7_U5TX);
GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);
UARTConfigSetExpClk(UART5_BASE, g_ui32SysClock, 57600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
IntMasterEnable();
IntEnable(INT_UART0); UARTIntEnable( UART0_BASE, UART_INT_RX | UART_INT_RT );
IntEnable(INT_UART5); UARTIntEnable( UART5_BASE, UART_INT_RX | UART_INT_RT );
while(1) {
// Loop for ever
}
}
I'm connecting PC to UART0 and my device to UART5 and if send
55 00 01 00 05 70 03 09 // in hex
I'm supposed to get
55 00 21 00 02 26 00 02 07 01 00 02 04 02 01 00 84 23 CC 45 4F 01 03 47 41 54 45 57 41 59 43 54 52 4C 00 00 00 00 00 A3 // in hex
But I'm getting
55 00 21 00 02 26 00 02 07 01 00 02 04 02 01 00 84 23 45 54 54 00
If I'm filling my lost data with XX, this will look like
55 00 21 00 02 26 00 02 07 01 00 02 04 02 01 00 84 23 XX 45 XX XX XX XX XX 54 XX XX XX XX XX 54 XX XX XX XX XX 00 XX XX
As you can see, after receiving some bytes, I'm constantly losing 5bytes of data in between.
Can anybody please help me to solve this problem?
Thanks,
vish