Other Parts Discussed in Thread: CDC5801A
Hello,
My customer needs to define the DCAN bit rate accuracy. Could you please advise?
- The final accuracy was not found in the DS or TRM.
- Therefore I'm trying to calculate from the clock path, but it is not successful.
I think the only error source is the PLL1 jitter. And the error will be reduced by dividers:
- The clock path is:
-
- Xtal: 16MHz +- 200ppm --> OSCIN
- PLL1: 160MHz
- VCLKA1 = DCAN clock input: 80MHz
- DCAN bit rate: 500kHz
Best regards,