This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Simple example of using hardware UART

I'm looking for a simple example of using the UART. I can find plenty of examples using the debugger virtual com port but I'm hoping to send the data out of PB0 and PB1. Can anybody link to where I should look? Thank you in advance.

  • Hi,

    How do you expect to do that? easy way or hard way?

    For "hard" way, which is not at all hard, look at, learn and test the uart_echo examples, and when ready just apply for PortB. To have communications with PC or other external device, you need also a level translator to be added to your hardware.

    The "easy" way - use PinMux utility to write some code for you - but try to avoid this... hope you need to learn some thing useful - better to read twice the user manual and driverlib source code.

    Petrei

  • Hello All,

    Or use one of the USB 2 UART dongles, reducing the chances of making a mistake doing a level translator.

    I agree there with Petrei, it is not the "hard" to retrofit one of the TivaWare examples for a new Pin/Peripheral Instance configuration.

    Regards

    Amit

  • Amit Ashara said:
    it is not "hard" to retrofit one of the TivaWare examples for a new Pin/Peripheral Instance configuration.

    Or not!

    Suppose one of the Port A instantiations is to be modeled.  Do not these "exploit" the default behavior of many of the Port A pins/peripherals?  And - via that default exploitation - the set-up/config code is somewhat reduced? 

    Then - when the user simply, "copies/pastes" (after tweaking to the new peripheral enumeration) that very available, Port A peripheral example code - as the set-up/config is "incomplete" - the "easy" retrofit fails!

    Imho all Port A code should be rewritten to include the normal/customary set-up/configs - required by any/all other peripheral instantiations!  Those Port A "shortcuts" have derailed many - and may thus conflict with the claim that retrofit is not, "hard."