Other Parts Discussed in Thread: TMDS570LS31HDK
Hi,
i connected the HDK board and gave the power supply and flashing some programs but it is not flashing and giving some target power loss error need to connect the usb emulator or turn on the power supply .i connected the powersupply and USB emulator also but it is not flashing wat's the problem
Can anyone help me (note:the ds2 & ds4 led is not glowing).
I checked the fuse F1(on top of it,it is written 150 F,24V), It is fine.
I checked the TP12 --> i'm getting 5V.
For TP14(1.2V) and TP16(3.3V) --> i'm getting 0V and 0.1V respectively.
I checked the right end of F1, it is giving me 12V.
Thanks,
Harsha