Hi,
I'm using CCS5.5, TMS570LS0332 and Halcogen 4.0.
I've set up SPI1 to have a baudrate of 1000kHz. However, the measured frequency is around 117kHz. I verified that if I drop the speed in Halcogen in half, the measured frequency drops in half as well.
What could cause the actual frequency not to match what it should? Is there some configuration I may have missed?
Thanks,
David