Hello,
I'm using DCC2 with the oscillator as Clock0 at 18MHz and HET2 pin 0 as Clock1 at 10KHz. Is there a limitation on the duty cycle of the PWM from the HET? Ideally, the duty cycle would be ~50%, but I want to also use the same instruction to generate an interrupt. I'd like to set a constant duty cycle somewhere between 5% and 95%.
Thanks, Charlie Johnston