This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD protection for ADC inputs



Hello,

Thank you for the reply.

I have some query regarding the ADC interface of microcontroller. i went through the datasheet and found the following internal block diagram for ADC pins.

From the diagram it is not clear what is the behaviour of the ADC pin for transient pulses. for eg. The ISO pulses will have maximum voltage of 100V. How the internal circuitry of ADC is protected or do we have to take this in to account in our circuit external to the microcontroller?

Kindly reply

Thanks

Kunmit