Sirs,
My customer is trying to read the pin#142 digital input state via the GIO register, but it is not successful. Could you please advice?
Customer test result
- The pin#142 state (Hi/Lo) didn't match the GIODINB[2] bit read. For example, regardsless the pin state the register output was one.
- GIO output was good. That is, the GIODOUTB[2] matched the pin#142 state. The problem was just readback.
- Tested with 2 customer boards. Both showed the phenomenon.
Remarks and questions:
- No findings in Errata as long as my study. I would appreciate your double-check. Chip revision-C.
- The TRM spnu499b is difficult for me in the following points. Your expalanation is highly appreciated:
- p228 Table 4-1: Does the pin#55 is used for GIOB[2] ?
- p228 Table 4-1: What is the right value for the PINMMR29[16] for GIOB[2] input usage?
- p241 Table 4-16: For register 0xFFFFEB34, "PINMMR9[18]" is not found but
we see "PINMMR29[16]". Is that correct?
Does PINMMR9[18] need to be configured?
Best regards,